cancel
Showing results for 
Search instead for 
Did you mean: 

MCU and Firmware package error while trying to generate the code using STM32CubeMX software

TH.16.336
Associate III
 
2 REPLIES 2

Hello @TH.16.336​ 

Please tell me which CubeMX version did you use.

I tried with the lasted CubeMX version(5.5.0) and it works correctly.

Best regards,

Nesrine

I am also using version 5.5.0.

Issue is with the network settings. If I download the package and give that repository path, then it's working fine.

But package downloading is not happening through CubeMX.