2019-12-16 3:36 PM
I have to configure OCTOSPI2 in Single Mode and only three pins managed directly from peripheral: SI, SO anche CLK.
The code generated from MX is the following:
static void MX_OCTOSPI2_Init(void)
{
...
OSPIM_CfgTypeDef OSPIM_Cfg_Struct = {0};
...
OSPIM_Cfg_Struct.ClkPort = 1;
OSPIM_Cfg_Struct.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
if (HAL_OSPIM_Config(&hospi2, &OSPIM_Cfg_Struct, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
Error_Handler();
}The function HAL_OSPIM_Config() checks validity of all members of OSPIM_Cfg_Struct:
HAL_StatusTypeDef HAL_OSPIM_Config(OSPI_HandleTypeDef *hospi, OSPIM_CfgTypeDef *cfg, uint32_t Timeout)
{
...
/* Check the parameters of the OctoSPI IO Manager configuration structure */
assert_param(IS_OSPIM_PORT(cfg->ClkPort));
assert_param(IS_OSPIM_PORT(cfg->DQSPort));
assert_param(IS_OSPIM_PORT(cfg->NCSPort));
assert_param(IS_OSPIM_IO_PORT(cfg->IOLowPort));
assert_param(IS_OSPIM_IO_PORT(cfg->IOHighPort));So this function fires an assert, because DQSPort and NCSPort are zero, but they should be 1 or 2.
Is this a bug in MX auto-generated code?
2020-01-28 7:45 AM
Hello @GModu.1 ,
I assume that the assert checks applied on HAL_OSPIM_Config (stm32l4xx_hal_ospi.c) should depend on the selected mode to configure the OctoSPI.
This is shared internally with our development team for further check & review.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.