2024-01-04 4:12 AM
Hello
we are using STM32H745XI Discovery board. When we are generating the project from CubeMX and opening in CubeIDE , the files are not generated properly. So that we can't build the project(check in attached png file)
--> it is not showing the build button.
we are tried in different versions of CubeIDE and CubeMX.
Help me in this regards
regards,
srikanth
2024-01-04 7:54 AM
Hello @Srikanth1,
I think the project is either not create or not imported correctly. Are you aware of the AN5361 named "Getting started with projects based on dual-core STM32H7 microcontrollers in STM32CubeIDE" ?
Best Regards,
Pierre
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.