cancel
Showing results for 
Search instead for 
Did you mean: 

If the libraries are linked in one system and I have to give it to another user(without him doing the"linking the library" process). How can I share the libraries of the projects? Automatically libraries should get linked in his system. How can I do that?

AKhot.1
Senior
1 REPLY 1
Semer CHERNI
ST Employee

Hello @AKhot.1​ 

First let me thank you for having reported.

The following thread is about a similar question https://community.st.com/s/question/0D50X0000BJ2gL4SQJ/how-to-add-external-libraries-in-stm32cubeide.

Feel free to repost in case the issue is not resolved.

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.