2018-10-18 5:18 AM
Hi,
I have some trouble to handle ADS7953 with HAL_SPI_TransmitReceive_DMA api,
if using HAL_SPI_TransmitReceive api, it takes long time and impact other operations,
so I hope to reduce the communication time with HAL_SPI_TransmitReceive_DMA in the communication of SPI, please help to let me know the method if possible, with detailed example,
I update my code, please help to review it, if finding something, please help to let me know what I should modify and how to modify with detailed example or explanation,
Thankful for your kindness in advance,
thanks.
My code is,
CS_Low;
if(HAL_SPI_TransmitReceive_DMA(&hspi2, cmd, data, 2) != HAL_OK) {
/* Transfer error in transmission process */
}
uint8_t state = HAL_SPI_GetState(&hspi2);
while (state != HAL_SPI_STATE_READY) {
state = HAL_SPI_GetState(&hspi2);
Hal_DebugPrint("SPI2_HS1_ManulMode hspi2 State is: %d\r\n", state);
}
CS_High;
and the setting case of SPI & DMA is,
/* USER CODE BEGIN SPI2_MspInit 0 */
/* USER CODE END SPI2_MspInit 0 */
__HAL_RCC_GPIOI_CLK_ENABLE();//love_0718
/* Peripheral clock enable */
__HAL_RCC_SPI2_CLK_ENABLE();
/**SPI2 GPIO Configuration
PI3 ------> SPI2_MOSI
PI2 ------> SPI2_MISO
PI1 ------> SPI2_SCK
*/
GPIO_InitStruct.Pin = GPIO_PIN_3|GPIO_PIN_2|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);
/* SPI2 DMA Init */
/* SPI2_TX Init */
hdma_spi2_tx.Instance = DMA1_Stream4;
hdma_spi2_tx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_tx.Init.Mode = DMA_NORMAL;
hdma_spi2_tx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi2_tx) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(hspi,hdmatx,hdma_spi2_tx);
/* SPI2_RX Init */
hdma_spi2_rx.Instance = DMA1_Stream3;
hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0;
hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_spi2_rx.Init.Mode = DMA_NORMAL;
hdma_spi2_rx.Init.Priority = DMA_PRIORITY_LOW;
hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
if (HAL_DMA_Init(&hdma_spi2_rx) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
__HAL_LINKDMA(hspi,hdmarx,hdma_spi2_rx);
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA1_Stream4_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn);
/* DMA interrupt init */
/* DMA1_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Stream3_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream3_IRQn);
thanks.
2018-10-19 8:26 AM
Hi @edmond yun ,
A detailed example is available under STM32Cube_FW_F4_V1.21.0\Projects\STM32F429I-Discovery\Examples\SPI\SPI_FullDuplex_ComDMA. It shows how to perform SPI data buffer transmission/reception between two boards via DMA.
HAL_SPI_TransmitReceive_DMA is used there.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-10-21 5:55 PM
Hello, @Amel NASRI ,
Firstly Thankful for your reply,
I would like to delivery what I did for this issue in a few days ago,
please help to refer it and to let me know the detailed example to solve this issue,
thankful for your support in advance,
frankly speaking, I don't know the method to use the example for ADS7953,
and I should use ADS7953 as a manual mode, can't probably use auto mode, I need to select the channel every time, in this case, I wonder whether DMA mode can't support ADS7953 in manual mode or not, please help to know your opinion for this question,
thanks.
2018-10-22 3:54 AM
Dear Edmond.
Did you want to communicate to Amel?.
Sorry to say that this is amelendez, not Amel NASRI.
Best regards.