How to disable USB Mass storage at runtime.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-23 10:15 AM
I to all,
I have a project where an STM32F013RTC use an SD card.
At run time the SD is share with FAT_FS or it is used as USB mass storage device, but not at the same time.
I need to disable USB module.
The configuration is made from CubeMX, so I have the function MX_USB_DEVICE_Init() to enable and configure USB.
void MX_USB_DEVICE_Init(void)
{
/* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */
/* USER CODE END USB_DEVICE_Init_PreTreatment */
/* Init Device Library, add supported class and start the library. */
if (USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS) != USBD_OK)
{
Error_Handler();
}
if (USBD_RegisterClass(&hUsbDeviceFS, &USBD_MSC) != USBD_OK)
{
Error_Handler();
}
if (USBD_MSC_RegisterStorage(&hUsbDeviceFS, &USBD_Storage_Interface_fops_FS) != USBD_OK)
{
Error_Handler();
}
if (USBD_Start(&hUsbDeviceFS) != USBD_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */
/* USER CODE END USB_DEVICE_Init_PostTreatment */
}
I wrote a function to disable USB:
void MX_USB_DEVICE_DeInit(void){
USBD_DeInit(&hUsbDeviceFS);
}
But this cause an Hard Fault reset.
Thre is an HAL function to disable USB module ?
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
STM32F1 Series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 3:12 PM
HI, I resolved the issue by using low level function provided from HAL:
void MX_USB_DEVICE_Stop(void){
USBD_LL_Stop(&hUsbDeviceFS);
}
void MX_USB_DEVICE_Start(void){
USBD_LL_Start(&hUsbDeviceFS);
}
I add this two in USB_device.c ( forv isibility of hUsbDeviceFS).
It works fine!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-23 8:22 PM
Perhaps debug the hard fault to determine the reason for the error.
HAL libraries are not created with robustness in mind, especially for uncommon scenarios.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-23 10:22 PM
Hi TDK,
Hard fault is rised at exit of this function
void MSC_BOT_DeInit(USBD_HandleTypeDef *pdev){
USBD_MSC_BOT_HandleTypeDef *hmsc = (USBD_MSC_BOT_HandleTypeDef *)pdev->pClassData;
hmsc->bot_state = USBD_BOT_IDLE;
}
It is called in USBD_MSC_DeInit();
uint8_t USBD_MSC_DeInit(USBD_HandleTypeDef *pdev,
uint8_t cfgidx){
/* Close MSC EPs */
USBD_LL_CloseEP(pdev, MSC_EPOUT_ADDR);
pdev->ep_out[MSC_EPOUT_ADDR & 0xFU].is_used = 0U;
/* Close EP IN */
USBD_LL_CloseEP(pdev, MSC_EPIN_ADDR);
pdev->ep_in[MSC_EPIN_ADDR & 0xFU].is_used = 0U;
/* De-Init the BOT layer */
MSC_BOT_DeInit(pdev);
/* Free MSC Class Resources */
if (pdev->pClassData != NULL)
{
USBD_free(pdev->pClassData);
pdev->pClassData = NULL;
}
return USBD_OK;
}
Every pointer used is not NULL.
For the scenarios, this is simply:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_USB_DEVICE_Init();
/* USER CODE BEGIN 2 */
MX_USB_DEVICE_DeInit();
I did this to avoid having to manually modify the code every time I change something in CubeMX (the project is still in the prototype phase)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 3:12 PM
HI, I resolved the issue by using low level function provided from HAL:
void MX_USB_DEVICE_Stop(void){
USBD_LL_Stop(&hUsbDeviceFS);
}
void MX_USB_DEVICE_Start(void){
USBD_LL_Start(&hUsbDeviceFS);
}
I add this two in USB_device.c ( forv isibility of hUsbDeviceFS).
It works fine!