2021-11-19 10:21 AM
I have a ethernet module "LAN8720" and I have STM32H743VIT8. But MCU has only "LAN8742" driver. Is it possible to add the "LAN8720" driver to the list of drivers?
2021-11-19 11:51 AM
You can take the driver from the ARM CMSIS collection, here.
2021-11-19 11:59 AM
Thank you for answer, and in what folder I have to put it for appear it in the list of "Driver_PHY"?
2021-11-19 2:08 PM
Put the .c and .h files in any place where you like.
Then add them to your project manually and call from your ethernetif.c.
Let the Cube/CubeIDE think that you use LAN8742.
2022-03-30 11:18 AM
The problem was solved?
2022-03-30 12:03 PM
No
2022-04-23 2:38 PM
> I have a ethernet module "LAN8720" and ... has only "LAN8742" driver.
For your code they are compatible. But there is a bug in CubeMX:
Also read this: