2020-02-19 12:25 AM
2020-02-19 05:42 AM
Hi,
Follow the instruction in the "STM32CubeMX for STM32 configuration and initialization C code generation" - User manual.
Regards
Imen
2020-02-25 02:21 AM
Hi,
thanks for your reply. I have already tried to follow the instruction. But it doesnt work, because of the damaged jar-file. Following error message popped up:
Error: Main class com.izforge.izpack.uninstaller.Uninstaller could not be found or load.
The other options dont work too. I am not able to uninstall this software.
Regards
MWale.1
2020-05-21 11:36 AM
I can't uninstall it also
2020-05-21 12:36 PM
Is it still unresolved? I have the same issue here.
2020-05-21 02:26 PM
That's it. I tried everything. If I don't hear from tech support, we don't use this.
2020-05-22 02:15 AM
@MWale.1
Open the cmd (run as administrator)
C:\windows\system32>java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.6.1\Uninstaller\uninstaller.jar" (Note : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.6.1\ is my cubeMX installation path)
Follow steps then it will be uninstalled.