cancel
Showing results for 
Search instead for 
Did you mean: 

How do I install and uninstall STM32CubeMX-5.5.0 silently from the command line?

MWale.1
Associate
 
6 REPLIES 6
Imen.D
ST Employee

Hi,

Follow the instruction in the "STM32CubeMX for STM32 configuration and initialization C code generation" - User manual.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
MWale.1
Associate

Hi,

thanks for your reply. I have already tried to follow the instruction. But it doesnt work, because of the damaged jar-file. Following error message popped up:

Error: Main class com.izforge.izpack.uninstaller.Uninstaller could not be found or load.

The other options dont work too. I am not able to uninstall this software.

Regards

MWale.1

John Winters
Associate III

I can't uninstall it also

Is it still unresolved? I have the same issue here.

John Winters
Associate III

That's it. I tried everything. If I don't hear from tech support, we don't use this.

Khouloud ZEMMELI
ST Employee

​@MWale.1​ 

Open the cmd (run as administrator)

C:\windows\system32>java -jar "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.6.1\Uninstaller\uninstaller.jar" (Note : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX-5.6.1\ is my cubeMX installation path)

Follow steps then it will be uninstalled.