cancel
Showing results for 
Search instead for 
Did you mean: 

FW_H7 V1.11.2 broke ADC configuration selections

GreenGuy
Lead

Ops!!!  The latest firmware does support internal channel selection on ADC3.

I verified that the previous firmware V1.11.1 gives visibility to the ADC3 internal channels for VBat, Temperature, and RBUF.  But if the firmware is migrated to V1.11.2 those selections disappear.

Screen shot from V1.11.2: After migration.

GreenGuy_0-1714508582404.png

Before migration (V1.11.1):

GreenGuy_1-1714508728898.png

 

I have also verified that starting a new project from scratch using any STM32H743 automatically applies V1.11.2 to start and once this happens, the internal channels are no longer available if if you change the firmware back to V1.11.1.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @GreenGuy,

Please download and use the latest patch release of STM32CubeMX v 6.11.1 which contains the fix.

ImenD_0-1714571216989.png

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

2 REPLIES 2
mÆŽALLEm
ST Employee

Hello,

It's an already known regression on CubeMx 6.11. 

See this thread: https://community.st.com/t5/stm32cubeide-mcus/h7-adc3-does-no-longer-offer-selection-for-temperature-after/m-p/652476

(internal ticket 176638)

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Imen.D
ST Employee

Hello @GreenGuy,

Please download and use the latest patch release of STM32CubeMX v 6.11.1 which contains the fix.

ImenD_0-1714571216989.png

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen