cancel
Showing results for 
Search instead for 
Did you mean: 

fsdata_custom.c missing in LWIP library for CubeMX 5.4.0 - How can I add it?

DMårt
Lead

Hi!

I trying to follow this manual to set upp a HTTPD web server in STM32 Nucleo H7 board. But I got a issue because fsdata_custom.c is missing and it seems that I cannot set HTTPD_USE_CUSTOM_FSDATA to false neither. Is this a bug in CubeMX?

How can I solve it? I posted a screen shot and it will give you all the information about my board I'm using. 0690X00000ArJYmQAN.png

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer
4 REPLIES 4
Mikhail Z
Senior II

See p.8 about the fsdata.c file.

That's about file fsdata.c, not fsdata_custom.c

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer
Mikhail Z
Senior II

Just change the filename in either place.

Gregory3
Associate III

Hello!

I'm also trying to get a simple ping answer from my STM32F767 according to start point pdf description. But with no results.

Could you please help me a little bit to understand the issue I have?

I have connected my custom board with LAN8742a with a Ethernet cable directly to my PC and just try to ping the Board.

I have disabled to whole HTTPD option, so I don't care abot the missing files for now.

My settings for the ETH are:

0693W000004KAMcQAO.png 

Nothing change for the PHY settings (default LAN8742a) and the interrupts are enabled. GPIOs are double checked.

My settings for the LwIP are:0693W000004KAMwQAO.pngAnd here is my main:

/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "lwip.h"
#include "gpio.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_LWIP_Init();
  /* USER CODE BEGIN 2 */
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
	  //Read a received packet from the Ethernet buffers and Send it to the lwIP stack for handling
	  MX_LWIP_Process();
  }
  /* USER CODE END 3 */
}

Any ideas what I'm doing wrong?

Regards,

Gregor