2021-01-19 5:36 PM
Editing C:\ST\STM32CubeIDE_1.0.2\STM32CubeIDE\plugins\com.st.stm32cube.common.mx_6.1.1.202012091304\db\templates\fatfs_platform_c.ftl
#include "fatfs_platform.h"
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
uint8_t BSP_PlatformIsDetected(void) {Above "USER CODE BEGIN Includes and END" section fixes it ... until new firmware package is available.
2021-01-19 11:32 PM
Hi @Community member ,
could you share your .ioc file ?
2021-01-20 11:42 AM
Can't share .ioc as it's a production version, but prepared to share the customized BSP_PlatformIsDetected() function.
The issue is we have 2 generations of board, using 1 common code set, and 1 .ioc file and 1 bin file
The difference between the boards is the SD Card detect pin moved.
The 'MK2' SD card detect pin is defined as SD_DETECT in the .ioc file and the MK1_SD_DETECT defined in an include file.
uint8_t BSP_PlatformIsDetected(void) {
uint8_t status = SD_PRESENT;
/* Check SD card detect pin */
if(HAL_GPIO_ReadPin(SD_DETECT_GPIO_PORT, SD_DETECT_PIN) != GPIO_PIN_RESET)
{
status = SD_NOT_PRESENT;
}
/* USER CODE BEGIN 1 */
/* user code can be inserted here */
if ( board.has_ade7953 == 0 ) {
if(HAL_GPIO_ReadPin(MK1_SD_DETECT_GPIO_PORT, MK1_SD_DETECT_PIN) != GPIO_PIN_RESET)
{
status = SD_NOT_PRESENT;
} else {
status = SD_PRESENT;
}
printf( "MK1_SD_DETECT: ");
} else {
printf( "MK2_SD_DETECT: ");
}
if ( status == SD_PRESENT ) {
printf( "Present\r\n");
} else {
printf( "Not present\r\n");
}
/* USER CODE END 1 */
return status;
}
2021-01-21 3:14 PM
@Houssem CHAABANIHopefully my last reply is enough to explain why we need the USER CODE BEGIN/END includes.
Note: Nick change, My old email provider closed down, so having to us a new login.
I wish this forum allowed changing email address in "My Profile".