STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1559 Views
  • 0 replies
  • 2 kudos

BUG: STM32CubeMX Task Stack Size, words Vs bytes.

The GUI interface for defining FreeRTOS tasks dictates that stack size is specified in words. That generates a call to CMSIS V2's osThreadNew() which requires attributes.stack_size to be specified in bytes. (The CMSIS layer then divides that by 4 to ...

0690X00000BxopVQAR.png

STM32CubeMX into stm32CubeIDE is very slow work!!!

hi :grinning_face: i tested several version of stm32CubeIDE for this,cubeMX inside stm32CubeIDE, is very slow working(exp: change pin name)but standalone stm32CubeMX, is normal work.Is there a solution to this? :\ #stm32CubeIDE #stm32CubeMX #stm32Cu...

kshin.111 by Associate III
  • 4890 Views
  • 8 replies
  • 0 kudos

I2C2 doesn't work

Hello, I am working with a custom board, using STM32F105VC. The board has some LED drivers, which they use I2C1 and I2C2. I2C1 works fine but I2C2 doesn't work. Configuration for both I2C are the same.  hi2c2.Instance = I2C2; hi2c2.Init.ClockSpeed = ...

NASI by Senior
  • 2017 Views
  • 2 replies
  • 0 kudos

STM32 CUBEMX v6.3.0 does not work with H7 firmware v1.8

I recently upgraded CubeMX to latest v6.3.0 and I have my project based on STM32H743IIT6 microcontroller. If I try to open my project which is made using H7 firmware v1.8 without migrating it to latest v1.9 then CubeMX gets hanged and its not able t...

VShet.2 by Associate III
  • 1951 Views
  • 3 replies
  • 0 kudos

Resolved! Hi I am concerned about the following microcontroller : STM32H753XIH6TR When using cube Mx to configure the timers on pin PA1_C the options specified in the data sheet are not avaliable. How do I access these functions?

Please see attatched image of functions specified in datasheet.Please see image attatched of functions avalailable on cube MXThanks for your help !

LMyle.1 by Associate III
  • 4759 Views
  • 11 replies
  • 1 kudos