2024-04-05 2:43 AM
Hi,
I would like to create a project with CubeMX where I handle files on a SD card with FAT Fs file system using a STM32U5 mcu.
When I select the STM32U5 MCU in CubeMX the FATFS middleware is not available, while If I select other MCUs series like STM32F for example the FATFS Middleware is available.
I tried to find the FATFS software package to manually install it into CubeMX but I haven't found nothing.
Is FATFS middleware available for STM32US MCUs for CubeMX ?
Thanks for your help.
2024-04-05 3:06 AM
Hello @jacopokunak ,
First let me thank you for posting and welcome to the ST Community.
I suggest please that you provide the STM32CubeMX version.
Thanks.
Mahmoud.
2024-04-05 3:09 AM
2024-04-05 3:12 AM
Hi,
It's CubeMX 6.11.0.
2024-04-05 3:21 AM
Thank you @Andrew Neil for linking that post.
From that discussion it seems like there is no intention from ST to support FATFS Middleware for STM32U5 MCUs in CubeMX at all am I right ?
If we want to use FATFS we need to get the source code from https://github.com/STMicroelectronics/stm32_mw_fatfs/tree/master include it in our projects and configure it manually ?
I do not want to use FileX in my project since it doesn't need to run with RTOS.
2024-04-05 3:33 AM
Hello @jacopokunak ,
In the STM32CubeU5 firmware, the file system has been migrated from FATFS to FileX.
I suggest that you to take a look at this POST in order to know more about it.
It demonstrates also how to develop a basic SD card file operations application.
Thanks.
2024-04-05 3:46 AM
@jacopokunak wrote:I do not want to use FileX in my project since it doesn't need to run with RTOS.
@Mahmoud Ben Romdhane does FileX require the use of the Azure® RTOS, or can it be used standalone?
2024-04-05 3:50 AM
It requires the use of AzureRTOS.
2024-04-05 3:52 AM
@Mahmoud Ben Romdhane wrote:In the STM32CubeU5 firmware, the file system has been migrated from FATFS to FileX.
I suggest that you to take a look at this POST in order to know more about it.
Following the FAQ link from that page, I got to this:
It's not very helpful to say, "refer to the relative ST Wiki page to get more information" when none of those Wiki pages exists!