2025-01-31 05:23 AM - edited 2025-02-04 11:42 PM
I'm using STM323H755ZIT6 NUCLEO board, STM32CubeMX 6.13.0 and STM32CubeIDE 1.17.0.
In my scenario, I created a project in STM32CubeMX 6.13.0 and generated the project. After that, I opened this project in STM32CubeIDE 1.17.0 and added paths for external folders in Paths and Symbols. Later, I edited the .IOC file in STM32CubeMX and tried to regenerate the project, but an error popup appeared.
After this popup, I clicked the OK button, and STM32CubeMX showed 'Project Successfully Generated.' However, when I tried to build the project in STM32CubeIDE, it failed to build, and errors appeared, such as:
D:/NAVANEETHAN/CoffeeMaker/DisplayControl/Project/DisplayControl/CM7/Core/Src/main.c:116: undefined reference to `HAL_Init'
D:/NAVANEETHAN/InstalledSoftwares/STM32CubeIDE_1.17.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe:
A total of 40 errors were shown, all related to HAL and OS kernel functions.
I attached All errors in Errors.txt
anyone support about this issue
Thank you
2025-01-31 05:26 AM
@NavaneethanN wrote:an error popup appeared.
It tells you to check that log file - so did you?
2025-01-31 06:04 AM
Hello @NavaneethanN
Could you provide your IOC file in order to further investigate the issue?
KR, Souhaib
2025-01-31 08:15 PM
Hi @Souhaib MAZHOUD
i attached the IOC file
2025-01-31 08:17 PM
@Andrew Neil
yeah, but i couldn't find anything bro