Skip to main content
Andrei Chichak
Lead
January 7, 2022
Solved

STM32CubeMX 6.4.0 doesn't interact nicely with MacOS 12.1 (Monterey)

  • January 7, 2022
  • 5 replies
  • 2515 views

CubeMX under Monterey seems to now think that all of my ioc files are read-only and not valid project files.

Also, when I <File><Load Project> no files or directories show up in my Documents directory.

This all worked before I updated to Monterey.

This topic has been closed for replies.
Best answer by Aymen CHAKROUN

Hi @Andrei Chichak​,

Ok, let's try a second solution.

I upload a video screen record showing the second method [tested OK in my environment].

The video => Enable_Full_access.7z

Waiting your feedback,

Regards,

Aymen.

5 replies

Aymen CHAKROUN
ST Employee
January 10, 2022

Hi @Andrei Chichak​ ,

Can you please apply the following solution extracted from the CubeMX UM1718:

0693W00000Hr5W6QAJ.png 

Let me know the result.

Regards,

Aymen.

Andrei Chichak
Lead
January 10, 2022

Hello @Aymen CHAKROUN​ ,

I'd have to say, no, this did not solve the problem.

I gave CubeMX full disk access, checked - still doesn't work, rebooted, checked - doesn't work. I installed 6.4.0 on windows in a vm under Fusion and it does work (even if I'm having problems downloading the firmware files from the ST repo).

Under windows, the file is not read-only and is valid. Under MacOS Monterey the file is read-only, invalid, then it is no longer visible in the file chooser dialog box. Going up a level in the directory structure does not show any files or directories.

If I create a new project in Cube, I can then save it and load it, but any previous projects are invalid, and very difficult to find as I can't navigate the file system through the dialog box.

(Also on the windows version, grep the code for the word "setted". I can't remember where I encountered it, something to do with download proxies, but that's not a word.)

Aymen CHAKROUN
Aymen CHAKROUNBest answer
ST Employee
January 11, 2022

Hi @Andrei Chichak​,

Ok, let's try a second solution.

I upload a video screen record showing the second method [tested OK in my environment].

The video => Enable_Full_access.7z

Waiting your feedback,

Regards,

Aymen.

Andrei Chichak
Lead
January 12, 2022

...IS THE CORRECT ANSWER!!!

Thank you @Aymen CHAKROUN​ , you are absolutely correct. My system preference pane had STM32CubeIDE and not STM32CubeMX.

The drag-drop that you show in your video was just what I needed.

Thank you again.

Andrei (from the great white north)

Remyhx
Associate III
February 15, 2025

Apparently still an issue in 2025 with CubeMX 6.13.0 and MacOS Sequoia. But thx, it worked!