cancel
Showing results for 
Search instead for 
Did you mean: 

Error[Lp015]: section placement failure caused by HAL_Unlock???

Taco!
Associate

Im using an F4 and modified my code to support an analog input using CubeMX. It messed up my project directory so i copied the new adc files to my unharmed project. I now get an "Error[Lp015]: section placement failure: overcommitted content in [0x802'0000-0x803'ffff]" and "Error while running Linker".

Part of the code in the auto generated adc.c file is a function called MX_ADC1_Init();

If i call this function i get the above error. If it is commented out, it builds successfully. If i call that function but comment everything out it builds successfully. If I incrementally add things in until i get the error then it fails within the HAL_ADC_Init() function (which is within the MX_ADC1_Init() function). Within the HAL_ADC_Init() function it fails when I uncomment hadc->Lock = HAL_UNLOCKED;

The code below shows the hadc->Lock = HAL_UNLOCKED as uncommented. Has anyone seen this before? What could cause it? How do I fix it?

Edit: worth noting is that many other unlock statements work correctly (ie: huart->Lock = HAL_UNLOCK, htim->Lock = ..., heth, hspi, hi2c, hrng, etc.)

HAL_StatusTypeDef HAL_ADC_Init(ADC_HandleTypeDef* hadc)
{
  HAL_StatusTypeDef tmp_hal_status = HAL_OK;
//  
//  /* Check ADC handle */
  if(hadc == NULL)
  {
    return HAL_ERROR;
  }
//  
//  /* Check the parameters */
  assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));
  assert_param(IS_ADC_CLOCKPRESCALER(hadc->Init.ClockPrescaler));
  assert_param(IS_ADC_RESOLUTION(hadc->Init.Resolution));
  assert_param(IS_FUNCTIONAL_STATE(hadc->Init.ScanConvMode));
  assert_param(IS_FUNCTIONAL_STATE(hadc->Init.ContinuousConvMode));
  assert_param(IS_ADC_EXT_TRIG(hadc->Init.ExternalTrigConv));
  assert_param(IS_ADC_DATA_ALIGN(hadc->Init.DataAlign));
  assert_param(IS_ADC_REGULAR_LENGTH(hadc->Init.NbrOfConversion));
  assert_param(IS_FUNCTIONAL_STATE(hadc->Init.DMAContinuousRequests));
  assert_param(IS_ADC_EOCSelection(hadc->Init.EOCSelection));
  assert_param(IS_FUNCTIONAL_STATE(hadc->Init.DiscontinuousConvMode));
//  
  if(hadc->Init.ExternalTrigConv != ADC_SOFTWARE_START)
  {
    assert_param(IS_ADC_EXT_TRIG_EDGE(hadc->Init.ExternalTrigConvEdge));
  }
//  
  if(hadc->State == HAL_ADC_STATE_RESET)
  {
//    /* Initialize ADC error code */
    ADC_CLEAR_ERRORCODE(hadc);
//    
//    /* Allocate lock resource and initialize it */
    hadc->Lock = HAL_UNLOCKED;   //THIS IS THE FAILURE POINT!!!!!!!!!!!!
//    
//    /* Init the low level hardware */
//    HAL_ADC_MspInit(hadc);
  }
//  
//  /* Configuration of ADC parameters if previous preliminary actions are      */ 
//  /* correctly completed.                                                     */
//  if (HAL_IS_BIT_CLR(hadc->State, HAL_ADC_STATE_ERROR_INTERNAL))
//  {
//    /* Set ADC state */
//    ADC_STATE_CLR_SET(hadc->State,
//                      HAL_ADC_STATE_REG_BUSY | HAL_ADC_STATE_INJ_BUSY,
//                      HAL_ADC_STATE_BUSY_INTERNAL);
//    
//    /* Set ADC parameters */
//    ADC_Init(hadc);
//    
//    /* Set ADC error code to none */
//    ADC_CLEAR_ERRORCODE(hadc);
//    
//    /* Set the ADC state */
//    ADC_STATE_CLR_SET(hadc->State,
//                      HAL_ADC_STATE_BUSY_INTERNAL,
//                      HAL_ADC_STATE_READY);
//  }
//  else
//  {
//    tmp_hal_status = HAL_ERROR;
//  }
//  
//  /* Release Lock */
//  __HAL_UNLOCK(hadc);
 
  /* Return function status */
  return tmp_hal_status;
}

4 REPLIES 4
Pavel A.
Evangelist III

> overcommitted content in [0x802'0000-0x803'ffff]"

So, is the program just growing more than 128K?

-- pa

Ozone
Principal

I agree - ssupposedly your code size grew beyond Flash size.

Check the linker map file, to see which objects seize that much space.

Piranha
Chief II

AMap - a nice tool to look at *.map files.

Atollic and Cube IDE have a similar tool, the Build Analyzer.

Open it after successful build. For best results, check "generate list file" in post-build outputs.

-- pa