cancel
Showing results for 
Search instead for 
Did you mean: 

Error Log: CubeMX plugin appears to be active, Log4j initialization might be too late.

BHime
Associate II

I am running STM32CubeIDE Version: 1.11.2 Build: 14494_20230119_0724 (UTC). When I startup CubeIDE, I am seeing the following error in the Error Log: 

"CubeMX plugin appears to be active, Log4j initialization might be too late."

I would appreciate it if someone could point me in the correct direction to resolve it (or ignore it). I am relatively new to CubeIDE, as I have primarily been doing my STM32 work from the command line with Makefiles. CubeIDE seems to be working fine so the error is not slowing me down at the moment.

9 REPLIES 9
BHime
Associate II

Additional information from the log file:

eclipse.buildId=Version 1.11.2

java.version=11.0.16

java.vendor=Eclipse Adoptium

BootLoader constants: OS=win32, ARCH=x86_64, WS=win32, NL=en_US

Command-line arguments: -os win32 -ws win32 -arch x86_64

Semer CHERNI
ST Employee

Hello @BHime​ 

First let me thank you for posting.

Could you provide the complete log files found under the "workspace\.metadata" directory:

  • .ide.log file
  • .log file

Kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

BHime
Associate II

Hi Semer,

Thanks for getting back to me on this issue. Here is the .log file.

BHime
Associate II

Here is the .ide.log file.

BHime
Associate II

Also, there is a .log4j.xml file that might be relevant.

Jiaming
Associate III

Hello, 

I encounter the same error. Not sure what happened? I am using stm32cubeide 1.14.1

Jiaming_0-1709125383062.png

 

mpX
Associate

Any solution on this problem?!, I have the same error message...

techdesk
Associate III

I have the same problem. Any solution yet?

wojciech239955
Associate II

I encounter the same error. I am using stm32cubeide 1.16.1