2025-01-22 10:17 AM
Hello,
I'm pretty new to this, but bear with me...
Generating configuration code for NUCLEO-H732FX which includes MEMS. In app_mems.c the generated code appears to attempt initializing the virtual COM out with an incorrectly formed call:
/* Initialize Virtual COM Port */
BSP_COM_Init(COM1);
returning:
the declaration in stm32h7xx_nucleo.c seems to confirm the incorrect call:
#if (USE_BSP_COM_FEATURE > 0)
/**
* @brief Configures COM port.
* @PAram COM COM port to be configured.
* This parameter can be COM1
* @PAram COM_Init Pointer to a UART_HandleTypeDef structure that contains the
* configuration information for the specified USART peripheral.
* @retval BSP error code
*/
int32_t BSP_COM_Init(COM_TypeDef COM, COM_InitTypeDef *COM_Init)
I suppose I could try editing the generated code, but any other workarounds that don't require editing would be greatly appreciated!
2025-01-23 12:40 AM - edited 2025-01-23 12:41 AM
Hello @TheMentat
First let me thank you for posting.
Are you sure about the board part number "NUCLEO-H732FX" ?
I would appreciate it if you could provide your IOC
I will be waiting for your feedback.
THX
Ghofrane
2025-01-28 6:55 AM
@TheMentat wrote:In app_mems.c the generated code appears to attempt initializing the virtual COM out with an incorrectly formed call:
How is COM1 defined?
It could be a macro, so it could define both parameters?