cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v6.12 generate wrong makefile project

Soraka
Associate

I use CubeMX + VSCode + arm-gcc + makefile to compile embedded programs. CubeMX v6.12 create wrong stm32fxxx_flash.ld file. Some words like "RAM" is lacked. And CubeMX v6.11 and CubeMX v6.10 is right.

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Hello @Soraka and welcome to the community,

Try the latest version 6.13 ..

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
mÆŽALLEm
ST Employee

Hello @Soraka and welcome to the community,

Try the latest version 6.13 ..

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks. I saw related answer in STM32CubeMX errata 6.12.x.

Did you test 6.13 and check if the behavior still there?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
toroid
Associate III

Had the same problem with a project using H7 series. I can confirm that updating CubeMX from 6.12 to 6.13 fixed the issue.