2024-11-27 02:03 AM
I use CubeMX + VSCode + arm-gcc + makefile to compile embedded programs. CubeMX v6.12 create wrong stm32fxxx_flash.ld file. Some words like "RAM" is lacked. And CubeMX v6.11 and CubeMX v6.10 is right.
Solved! Go to Solution.
2024-11-27 02:04 AM - edited 2024-11-27 02:07 AM
Hello @Soraka and welcome to the community,
Try the latest version 6.13 ..
2024-11-27 02:04 AM - edited 2024-11-27 02:07 AM
Hello @Soraka and welcome to the community,
Try the latest version 6.13 ..
2024-11-27 02:05 AM
v6.13.0 has just been released:
https://community.st.com/t5/stm32cubemx-mcus/stm32cubemx-6-13-0-released/td-p/747679
Have you tried it?
2024-11-27 02:28 AM
Thanks. I saw related answer in STM32CubeMX errata 6.12.x.
2024-11-27 02:33 AM
Did you test 6.13 and check if the behavior still there?
2024-12-18 04:48 AM
Had the same problem with a project using H7 series. I can confirm that updating CubeMX from 6.12 to 6.13 fixed the issue.