cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX - STM32F3

George.P
Associate III
Posted on September 17, 2014 at 09:00

At the moment it seems that Cube for STM32F3  prepares only the

gpio

 files and calls 

MX_GPIO_Init

in main, unless I'm doing something terribly wrong.

Are there plans to generate peripheral support libraries and FreeRTOS in a close future update?

#stm32f3 #cubemx
2 REPLIES 2
Amel NASRI
ST Employee
Posted on September 18, 2014 at 11:59

Hello GeorgeP,

Which CubeMX version are you using? Last one is 4.3 and is totally supporting F3 products so that it can generate initialization code for all selected peripherals.

Please check again.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

George.P
Associate III
Posted on September 24, 2014 at 16:22

Hi Mayla,

Indeed I was using 4.0.0!

Now Cube has support for F3 and the Discovery Boards too!

Great stuff!

Thanks for the heads up :)