cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX " Not a valid ioc file" error

Adole.1
Associate

Hi,

I have installed STM32CubeMX v6.7 on my laptop. The installation was successful.

Loaded a project which was setup with STM32CubeMX v6.3 using FW_GO v1.5.0.

The code is generated successfully, however when pressing to open the project, " Not a valid ioc file" errors on the screen.

Attached STM32CubeMX log file.

Any idea how to resolve it ?

3 REPLIES 3
Pavel A.
Evangelist III

Do you have several STM32CubeMX versions installed? v6.7 and 6.3?

Adole.1
Associate

No, only v6.7​

Hi @Adole.1​,

Did you try with different ioc files?

How do you proceed: open the ioc with STM32CubeMX? or via STM32CubeIDE?

Make sure to install properly the CubeMX tool and STM32CubeG0 MCU package.

Can you please share you ioc file, to check this behavior?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen