2019-06-02 10:42 AM
Generated code for F429 Nucleo with USB CDC fails to compile Src\freertos.c etc. with messages:
..\Src\usb_device.c:55:22: fatal error: usbd_cdc.h: No such file or directory
..\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Src\usbd_cdc.c:62:22: fatal error: usbd_cdc.h: No such file or directory
In file included from ..\Src\usb_device.c:56:0:
../Inc/usbd_cdc_if.h:59:22: fatal error: usbd_cdc.h: No such file or directory
I've attached IOC for easy reproduction of bug.
Thanks for any help or bugfix,
Best Regards, Dave
PS: Attention @Markus GIRDLAND @Imen DAHMEN
2019-06-03 2:40 AM
Hello @Dave Nadler ,
Probably, the Include Paths is not set up properly or you are missing an include file
Go to Project options and add new paths to your include directories
Regards,
Imen
2019-06-03 5:24 AM
Thanks @Imen DAHMEN - Path Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Inc was missing.
Please confirm you've reproduced this bug, and this bug is in your queue to fix,
Best Regards, Dave
2019-06-17 3:26 AM
Hi @Dave Nadler ,
This issue is confirmed and will be fixed in the coming release of STM32CubeMX.
Thank you for highlighting this.
Best Regards
Imen
2020-07-29 9:10 PM
V6.0 Cube MX and STM32Cube IDE V1.40 still has this problem.
After adding Path Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Inc.
I still get errors "No such file or directory"
../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.c:21:10: fatal error: usbd_core.h: No such file or directory
../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ctlreq.c:21:10: fatal error: usbd_ctlreq.h: No such file or directory
../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ioreq.c:21:10: fatal error: usbd_ioreq.h: No such file or directory
../Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.c:21:10: fatal error: usbd_core.h: No such file or directory
2020-07-30 7:26 AM
@JP19 These files are in STM32_USB_Device_Library/Core/Inc/
-- pa