2024-12-17 5:10 AM - edited 2024-12-18 5:10 AM
I've been trying several days to just get any project up and going for the STM32WBA52GU. As soon as I add the WPAN middleware, the HAL definitions go haywire with errors when I compile it. I've tried following tutorial in the wiki with documentation, but nothing seems to be working. I can import an example for the Nucleo WBA55, and it will compile. However, using the same settings for a new project fails (even when trying to target the WBA55). Any help would be appreciated. I'm using STMCubeIDE 1.17.0 with the latest firmware libraries.
786 | HAL_StatusTypeDef HAL_RCCEx_PeriphCLKConfig(const RCC_PeriphCLKInitTypeDef *PeriphClkInit);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2452:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2452 | HAL_StatusTypeDef HAL_RCC_DeInit(void);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2453:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2453 | HAL_StatusTypeDef HAL_RCC_OscConfig(const RCC_OscInitTypeDef *RCC_OscInitStruct);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2454:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2454 | HAL_StatusTypeDef HAL_RCC_ClockConfig(const RCC_ClkInitTypeDef *RCC_ClkInitStruct, uint32_t FLatency);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rcc.h:2491:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_CRC_StateTypeDef'?
2491 | HAL_StatusTypeDef HAL_RCC_GetConfigAttributes(uint32_t Item, uint32_t *pAttributes);
| ^~~~~~~~~~~~~~~~~
| HAL_CRC_StateTypeDef
In file included from ../Core/Inc/stm32wbaxx_hal_conf.h:279:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:89:3: error: unknown type name 'HAL_LockTypeDef'
89 | HAL_LockTypeDef Lock; /*!< RNG locking object */
| ^~~~~~~~~~~~~~~
In file included from ../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:287:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:221:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
221 | HAL_StatusTypeDef HAL_RNGEx_SetConfig(RNG_HandleTypeDef *hrng, const RNG_ConfigTypeDef *pConf);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:222:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
222 | HAL_StatusTypeDef HAL_RNGEx_GetConfig(RNG_HandleTypeDef *hrng, RNG_ConfigTypeDef *pConf);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:223:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
223 | HAL_StatusTypeDef HAL_RNGEx_LockConfig(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng_ex.h:232:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
232 | HAL_StatusTypeDef HAL_RNGEx_RecoverSeedError(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:296:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
296 | HAL_StatusTypeDef HAL_RNG_Init(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:297:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
297 | HAL_StatusTypeDef HAL_RNG_DeInit(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:318:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
318 | HAL_StatusTypeDef HAL_RNG_GenerateRandomNumber(RNG_HandleTypeDef *hrng, uint32_t *random32bit);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:319:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
319 | HAL_StatusTypeDef HAL_RNG_GenerateRandomNumber_IT(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rng.h:369:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RNG_StateTypeDef'?
369 | HAL_StatusTypeDef RNG_RecoverSeedError(RNG_HandleTypeDef *hrng);
| ^~~~~~~~~~~~~~~~~
| HAL_RNG_StateTypeDef
In file included from ../Core/Inc/stm32wbaxx_hal_conf.h:283:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc.h:205:3: error: unknown type name 'HAL_LockTypeDef'
205 | HAL_LockTypeDef Lock; /*!< RTC locking object */
| ^~~~~~~~~~~~~~~
In file included from ../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc.h:732:
../Drivers/STM32WBAxx_HAL_Driver/Inc/stm32wbaxx_hal_rtc_ex.h:1487:1: error: unknown type name 'HAL_StatusTypeDef'; did you mean 'HAL_RTCStateTypeDef'?
1487 | HAL_StatusTypeDef HAL_RTCEx_SetTimeStamp(RTC_HandleTypeDef *hrtc, uint32_t TimeStampEdge, uint32_t RTC_TimeStampPin);
| ^~~~~~~~~~~~~~~~~
| HAL_RTCStateTypeDef
2024-12-19 7:43 AM
Hello @JLReyno ,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-12-19 10:06 AM
Thanks, Mahmoud! To keep you up to date with my latest work, I've tried some other advice and started with the P2P_server example for the WBA55 and then modified it for the WBA52. I can get it to compile, but the BLE stack fails to initialize (line 1081 in app_ble.c). I've attached that project for reference if that is any help.