2021-07-04 3:26 AM
Dear All, As you know well STM32CubeMX IDE is showing clock configuration block diagram which is the user programmable interface as showing in the attached picture. My question is ....Can we able to see all the timer block diagrams also in the format of clock configuration
Please advice
2021-07-04 8:47 AM
Any Help please
2021-07-04 12:38 PM
There's a block diagram of the timers at the beginning of all TIM chapters in the Reference Manual. Then there are detailed diagrams of the input and output stages of the Capture-Compare unit further in to the chapter.
Read it.
JW
2021-07-05 9:23 PM
Hi
waclawek.jan ,Grate thanks for the reply
It would be grate if I have animation level Timers like STM32CubeMX IDE is showing clock configuration block diagram
Thanks