cancel
Showing results for 
Search instead for 
Did you mean: 

Are there known problems with STM32CUBEMX 6.6.1 using USB_OTG and SDIO?

Barry Richards
Associate III

I have a custom board using a STM32F446RET6 with a SD micro card slot.

The card is formatted to exFAT with one partition.

Using STM32CUBEMX V6.6.1 with firmware F4 V1.27.1

For testing I have a minimal configuration as follows:

SDIO

  Mode SD 4 bits Wide bus

  DMA enabled for RX and TX

  SDIOCLOCK divide set to 4

  SDIO global interrupt enabled

USB_OTG_FS

  Mode is Device Only

  USB OTG global interrupt enabled

USB_DEVICE

  Class for FS IP = Mass Storage Class

  MSC_MEDIA_PACKET size is 512 bytes (I have tried increasing this)

MCU

  clock 168 MHz

  using 12 MHz external crystal

  SDIO clock is 48 MHz

  USB clock 48 MHz

Running this setup when I plug a usb cable to the board the following shows in the log:

usb 2-1.6: new full-speed USB device number 67 using ehci-pci

usb 2-1.6: New USB device found, idVendor=0483, idProduct=572a, bcdDevice= 2.00

usb 2-1.6: New USB device strings: Mfr=1, Product=2, SerialNumber=3

usb 2-1.6: Product: STM32 Mass Storage

usb 2-1.6: Manufacturer: STMicroelectronics

usb 2-1.6: SerialNumber: 207433514638

usb-storage 2-1.6:1.0: USB Mass Storage device detected

scsi host7: usb-storage 2-1.6:1.0

scsi 7:0:0:0: Direct-Access    STM     Product         0.01 PQ: 0 ANSI: 2

sd 7:0:0:0: Attached scsi generic sg4 type 0

sd 7:0:0:0: [sdd] 65536 512-byte logical blocks: (33.6 MB/32.0 MiB)

sd 7:0:0:0: [sdd] Write Protect is off

sd 7:0:0:0: [sdd] Mode Sense: 22 00 00 00

sd 7:0:0:0: [sdd] Write cache: disabled, read cache: enabled, doesn't support DPO or FUA

sd 7:0:0:0: [sdd] Attached SCSI removable disk

The logical blocks is incorrect, should be more like 15126528 512-byte logical blocks: (7.74 GB/7.21 GiB)

  which is what is reported using the same sdcard but a commercial adapter in my computer.

It also does not find the partition.

I believe my pcb is ok because with my full configuration using FATFS I am able to open the SD card and read files etc from it.

0 REPLIES 0