cancel
Showing results for 
Search instead for 
Did you mean: 

After upgrading CubeMx plugin from 6.10.0 to 6.11.0, MCU temperature sensor is no longer supported

TechGuyMike
Associate III

I'm using STM32CubeIDE and targeting STM32H745IIK6.  When I was using the CubeMx plugin version 6.10.0, I was able to enable the temperature sensor input on ADC3:

TechGuyMike_0-1713381591538.png

After upgrading to CubeMx 6.11.0 with FW package H7_v1110.zip, this option (as well as the two inputs listed immediately before and immediately after it) are now gone:

TechGuyMike_1-1713381627753.pngTechGuyMike_2-1713381648261.png

With upgraded SW/FW:

TechGuyMike_4-1713381786622.png

The three options that used to be listed towards the end of the page, between the "IN16" input and the "EXTI Conversion Trigger" are missing. Are they available elsewhere now?

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

This is a known regression in CubeMx.

See this thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

This is a known regression in CubeMx.

See this thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello,

Would you mind adding this issue to the errata page for CubeIDE (https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.15.0#STM32H7) or CubeMx (https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32CubeMX_errata_6.11.x)?


I've escalated this point and will get back to you for any new feedback.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.