cancel
Showing results for 
Search instead for 
Did you mean: 

Adding Additional Software Pack ARM.CMSIS 5.6.0 onSTM32H743, running on Nucleo H743ZI2, I get 'Incomplete Inclusion' error on all source files - Middleware folder.

MLane.3
Associate II

Every time, I regenerate the code after including the above ARM file, I get an error on all source files that states 'incomplete inclusion' - enable CMSIS DSP. I have been getting around this by adding the appropriate ARM DSP libraries manually. It is a little painful and eventually would like this error resolved?

5 REPLIES 5
Khouloud ZEMMELI
ST Employee

Hello @MLane.3​ 

Could you please share your ioc file?

Thanks

Khouloud

MLane.3
Associate II

here is the ioc file

Thanks @MLane.3​ for the feedback, issue will be fixed if you generate a keil project, in fact, this's not a CubeMX issue, it's a specific problem with ARM packs and we are sorry for that... so It's not possible to fix the issue from MX side as the RTE_components.h can be generated by CubeMX, only if there is some RTE_components into the PDSC .

For the choosen component , there is no RTE element

https://www.keil.com/pack/doc/CMSIS/Pack/html/pdsc_components_pg.html#RTE_Components_h

Best Regards

Khouloud

MLane.3
Associate II

... so bottom line; this does not work with STM32CubeIDE?

Sorry but no.

Regards,

Khouloud