Skip to main content
MFolk.1
Senior
January 30, 2024
Solved

MxCube Bug: STM32H747XI USB_HS includes API's in both projects

  • January 30, 2024
  • 4 replies
  • 1967 views

When attempting to configure USB_OTG_HS and corresponding USB_DEVICE_M4/M7 middleware on STM32H747XI (on either M7 or M4 cores), the "STM32_USB_Device_Library" directory gets included on both cores, causing the core that isn't using the USB peripheral to fail build. Here are the errors that occur:

/.../H7/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.c:20:10: fatal error: usbd_core.h: No such file or directory
20 | #include "usbd_core.h"
| ^~~~~~~~~~~~~
compilation terminated.
/.../H7/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ctlreq.c:20:10: fatal error: usbd_ctlreq.h: No such file or directory
20 | #include "usbd_ctlreq.h"
| ^~~~~~~~~~~~~~~
compilation terminated.
/.../H7/Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ioreq.c:20:10: fatal error: usbd_ioreq.h: No such file or directory
20 | #include "usbd_ioreq.h"
| ^~~~~~~~~~~~~~
compilation terminated.
/.../H7/Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/usbd_cdc.c:59:10: fatal error: usbd_cdc.h: No such file or directory
59 | #include "usbd_cdc.h"
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/ST/STM32_USB_Device_Library/Core/Src/subdir.mk:25: Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_core.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Middlewares/ST/STM32_USB_Device_Library/Core/Src/subdir.mk:27: Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ctlreq.o] Error 1
make: *** [Middlewares/ST/STM32_USB_Device_Library/Core/Src/subdir.mk:29: Middlewares/ST/STM32_USB_Device_Library/Core/Src/usbd_ioreq.o] Error 1
make: *** [Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/subdir.mk:19: Middlewares/ST/STM32_USB_Device_Library/Class/CDC/Src/usbd_cdc.o] Error 1
"make -j24 all" terminated with exit code 2. Build might be incomplete.

15:38:03 Build Failed. 9 errors, 0 warnings. (took 277ms)

This topic has been closed for replies.
Best answer by Ghofrane GSOURI

Hello @MFolk.1 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:172326(This is an internal tracking number and is not accessible or usable by customers).

For the moment in order to build the project successfully , you need to delete the ST folder under potentalH7_CM4\ Middlewares.

I will keep you posted with updates.

Thx

Ghofrane

4 replies

Ghofrane GSOURI
ST Technical Moderator
January 31, 2024

Hello @MFolk.1 

First let me thank you for posting.

I tried to reproduce the issue mentioned above using the latest version of CubeMX 6.10.0 and everything works correctly , could you please share your IOC in order to push further the investigation.

I will be waiting for your feedback.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MFolk.1
MFolk.1Author
Senior
January 31, 2024

Thanks for your willingness to look into this issue. See attached.

Note that I'm also using CubeMx 6.10.0 (within STM32CubeIDE 1.14.0).

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
February 1, 2024

Hello @MFolk.1 

Thank you for your contributions and for your detailed explanations,

I confirm the issue on my side, it has been reported to STM32CubeMX development team .

Internal ticket number:172326(This is an internal tracking number and is not accessible or usable by customers).

For the moment in order to build the project successfully , you need to delete the ST folder under potentalH7_CM4\ Middlewares.

I will keep you posted with updates.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.