2020-08-05 11:53 AM
Every time, I regenerate the code after including the above ARM file, I get an error on all source files that states 'incomplete inclusion' - enable CMSIS DSP. I have been getting around this by adding the appropriate ARM DSP libraries manually. It is a little painful and eventually would like this error resolved?
2020-08-06 1:50 AM
Hello @MLane.3
Could you please share your ioc file?
Thanks
Khouloud
2020-08-06 3:59 PM
2020-08-07 1:13 AM
Thanks @MLane.3 for the feedback, issue will be fixed if you generate a keil project, in fact, this's not a CubeMX issue, it's a specific problem with ARM packs and we are sorry for that... so It's not possible to fix the issue from MX side as the RTE_components.h can be generated by CubeMX, only if there is some RTE_components into the PDSC .
For the choosen component , there is no RTE element
https://www.keil.com/pack/doc/CMSIS/Pack/html/pdsc_components_pg.html#RTE_Components_h
Best Regards
Khouloud
2020-08-07 2:01 PM
... so bottom line; this does not work with STM32CubeIDE?
2020-08-10 1:06 AM
Sorry but no.
Regards,
Khouloud