Every time, I regenerate the code after including the above ARM file, I get an error on all source files that states 'incomplete inclusion' - enable CMSIS DSP. I have been getting around this by adding the appropriate ARM DSP libraries manually. ...
With the latest version of CubeMX (Version: 6.0.0-RC5) there is a reported error with ADC configuration. I will attached the preferred configuration below. The problem is that the latest version will not let me select ADC2, see attached configurati...
I would like to get examples of how to use the DTCM and ITCM per AN4891. I am particularly interested in examples of the configurations defined in AN4891- 1 - D1_ITCM - D1_DTCM, D1_ITCM - D1_AXISRAM and D1_ITCM - D1_SRAM.
Do you have an example? At least when using Stm32CubIde, it recommends not changing the linker as it is auto generated. Does that mean it needs to be setup in CubeMx or CubeIde?
Cheers
Mark
Get Outlook for iOS<></>