cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE sample program compiling error

nh7
Associate II

Hi,

I try to compile "OpenAMP_TTY_echo_CM33_NonSecure" sample program as suggested here:

https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-DK/Develop_on_Arm_Cortex-M33/Modify,_rebuild_and_reload_the_firmware

Compiling does not work, I get error message:

 

0:43:14 **** Build of configuration CA35TDCID_m33_ns_sign for project OpenAMP_TTY_echo_CM33_NonSecure ****

make -j16 all

cmake -S ../../../../../../../../../Middlewares/Third_Party/OpenAMP/libmetal/ -B libmetal -G"Unix Makefiles" -DCMAKE_TOOLCHAIN_FILE=cmake/platforms/stm32mp-generic-gcc.cmake

CMake Error at CMakeLists.txt:1 (cmake_minimum_required):

-- Configuring incomplete, errors occurred!

Compatibility with CMake < 3.5 has been removed from CMake.

 

Update the VERSION argument <min> value. Or, use the <min>...<max> syntax

to tell CMake that the project requires at least <min> but has been updated

to work with policies introduced by <max> or earlier.

 

Or, add -DCMAKE_POLICY_VERSION_MINIMUM=3.5 to try configuring anyway.

 

 

make[1]: *** [makefile:104: pre-build] Error 1

make: *** [makefile:72: all] Error 2

"make -j16 all" terminated with exit code 2. Build might be incomplete.

 

10:43:15 Build Failed. 2 errors, 0 warnings. (took 626ms)

 

-------------------

 

I have cmake 4.0.2 installed. I tried in Ubuntu and Windows, same error.

Can you please help?

 

 

1 REPLY 1
HimanshuT
ST Employee

Hi @nh7 ,

You can add argument as  -DCMAKE_POLICY_VERSION_MINIMUM=3.5 to the command as shown in the error or you can use cmake version 3.XX (For example 3.31.6).