2021-07-05 02:12 AM
When trying to create a new project with the NUCLEO-G474RE board I regularly get the error in the attached image. The project then consists of only the .ioc file and Cube crashes when trying to generate code.
Note that I have no issues creating a project for the NUCLEO-L496ZG board for example.
Solved! Go to Solution.
2021-07-05 03:44 AM
Hello @Matthias Noé ,
This seems like a network issue. Could you download the package directly from here https://www.st.com/en/embedded-software/stm32cubeg4.html and install it manually.
Best regards,
@SBEN .2
2021-07-05 03:44 AM
Hello @Matthias Noé ,
This seems like a network issue. Could you download the package directly from here https://www.st.com/en/embedded-software/stm32cubeg4.html and install it manually.
Best regards,
@SBEN .2
2021-07-06 02:12 AM
Hello @SBEN .2 ,
thank you for the advice and the link. I had no issues downloading the package.
I am using the following guide: https://www.st.com/resource/en/user_manual/dm00550255-getting-started-with-stm32cubeg4-for-stm32cubeg4-series-stmicroelectronics.pdf
However, when trying to set up an example project I seem to have difficulties following the instructions given on pg. 16.
What is meant by the "STM32CubeIDE workspace directory"?
I tried it with \Examples\GPIO\GPIO_EXTI\STM32CubeIDE but no project showed up when I tried to import. I think I am missing something.
Best regards,
Matt
2021-07-06 05:18 AM
Hello @Matthias Noé ,
As a shortcut, you can open the project's file and double click on the .cproject file. If the file association is correct, the workspace should be loaded immediately.
Best regards,
@SBEN .2
2021-07-06 05:41 AM
Thank you @SBEN .2
It all works fine now.