cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.6.0 released

mattias norlander
ST Employee

STM32CubeIDE 1.6.0 was released this week on st.com as well as a in-tool update patch.

Caution: The in-tool update does not allow updating drivers and ST-LINK server tool. Full installer is required for this.

What is new in 1.6.0? (only some highlights)

  • Target support updated in-sync with STM32Cube ecosystem in general. In particular:
    • Added support for additional STM32G0 and STM32WB series devices.
  • Integration of STM32CubeMX 6.2.0, STM32CubeProgrammer 2.7.0 and latest versions of various other STM32 deliverables.
  • Added Azure RTOS ThreadX debug support.
  • Toolchain manager changes
    • The Arm and Gnu Tools for STM32 toolchains based on GCC 9-2020-q2​ is the new default bundled and used toolchain in CubeIDE 1.6.0.
    • Toolchain manager extended to support using a locally installed 3rd party GCC toolchain.
  • Information Center updated with new Tools Panel for easy access/download of additional tools.
  • STM32CubeMX plug-in provides pinout compatible search feature
  • For MPU series :
    • Application / Library user land development
  • JRE updates
    • Moved to Java11
    • JRE is now distributed as plug-in allowing also in-tool update of JRE via P2

Main issues fixed in STM32CubeIDE 1.6.0

Only a sub-set of the many tickets closed are mentioned in the release note.

Known problems and limitations

Please refer to the release note.

Where do I Obtain CubeIDE 1.6.0?

  • https://www.st.com/stm32cubeide
  • ... Or update your current installation of STM32CubeIDE using: Help > Check for updates
    • Caution: After updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.
62 REPLIES 62

Late package which is same as early one according @mattias norlander​ is:

0693W000008vrZ0QAI.jpgJust rely on Help > About in case you need to be comfortable about.

My snapshot is based on fresh install I've done relying on www.st.com today

EGit works for me.

Looks pretty annoying indeed...

What is your OS?

Also could you share you workspace log file workspace/.metadata/.log to see if something guides us to the root cause?

OS - WIN10

Hi Markus,

I sent you the Log via private message yesterday. Thanks in advance.

OS is win10.

Thanks for sharing. In the light of such could you have a try starting a new IDE session but electing a brand new repository as workspace ? (possibly then just perform File > Open Project From File System to get bqck within such fresh workspace one of your project). I've feeling we have to exclude local corrupted workspace option here.

Please share back outcomes.

Thanks for sharing. In the light of such could you have a try starting a new IDE session but electing a brand new repository as workspace ? (possibly then just perform File > Open Project From File System to get bqck within such fresh workspace one of your project). I've feeling we have to exclude local corrupted workspace option here.

Please share back outcomes.

---

I'm sorry, I don't want to spend more time solving this. I want to work on my project so I installed 1.5.1 which works without problems.