cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.6.0 released

mattias norlander
ST Employee

STM32CubeIDE 1.6.0 was released this week on st.com as well as a in-tool update patch.

Caution: The in-tool update does not allow updating drivers and ST-LINK server tool. Full installer is required for this.

What is new in 1.6.0? (only some highlights)

  • Target support updated in-sync with STM32Cube ecosystem in general. In particular:
    • Added support for additional STM32G0 and STM32WB series devices.
  • Integration of STM32CubeMX 6.2.0, STM32CubeProgrammer 2.7.0 and latest versions of various other STM32 deliverables.
  • Added Azure RTOS ThreadX debug support.
  • Toolchain manager changes
    • The Arm and Gnu Tools for STM32 toolchains based on GCC 9-2020-q2​ is the new default bundled and used toolchain in CubeIDE 1.6.0.
    • Toolchain manager extended to support using a locally installed 3rd party GCC toolchain.
  • Information Center updated with new Tools Panel for easy access/download of additional tools.
  • STM32CubeMX plug-in provides pinout compatible search feature
  • For MPU series :
    • Application / Library user land development
  • JRE updates
    • Moved to Java11
    • JRE is now distributed as plug-in allowing also in-tool update of JRE via P2

Main issues fixed in STM32CubeIDE 1.6.0

Only a sub-set of the many tickets closed are mentioned in the release note.

Known problems and limitations

Please refer to the release note.

Where do I Obtain CubeIDE 1.6.0?

  • https://www.st.com/stm32cubeide
  • ... Or update your current installation of STM32CubeIDE using: Help > Check for updates
    • Caution: After updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.
62 REPLIES 62
mattias norlander
ST Employee

The thread is growing... It is becoming hard to follow the discussion both for support-team and end-users.

Feel free to reply to already identified issues in this thread.

But - please submit any new issue/feedback in new threads. Thanks!

Hi,

I am also facing the same issue, any resolution for the same.0693W000008y6GHQAY.pngRegards

Sai Ram Mannar

When you say "Play" what is the fix. Shouldn't it work by default on the nucleo board and which bit needs correcting as its now broken.

I'm happy to "play" but really we should know the exact correction as it could affect other things.

Thanks,

Mark