2023-09-19 09:29 AM
STM32CubeIDE 1.13.2 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.2 that is available for download.
Main issues fixed in this patch:
Where do I obtain STM32CubeIDE 1.13.2?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-21 03:09 AM
And no, it's not fixed.
It still opens an additional file at the 2nd start.
Also with a new workspace.
Werner
2023-09-26 11:33 PM
@Semer CHERNI On macos can't type '@' (alt + L) because it is hard coded to 'Login'. At least I can't find it on the list Preferences->General->Keys. Well, it is shown in csv if I export the list, but I can't find it on the list where I can change the bindings.
2023-10-20 06:06 PM - edited 2023-10-20 06:08 PM
In 1.13.2, when double-clicking with the mouse to prepare setup data, such as prescaler, a 'c' character often appears in the input box.