cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.13.2 released

Semer CHERNI
ST Employee

STM32CubeIDE 1.13.2 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.2 that is available for download.

Main issues fixed in this patch:

  • Ticket 160463 - [STM32CubeIDE 1.13.0]Build error after calling printf.
  • Ticket 160729 - [STM32CubeIDE] Update GCC binaries
  • Ticket 159568 - [DOC] Update the RN for 1.13.2
  • Ticket 158617 - [STM32H745][STM32CubeIDE][1.13.0][Headless build] - H745 Build fails on latest CubeIDE

Where do I obtain STM32CubeIDE 1.13.2?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 REPLIES 3
padawan
Senior

And no, it's not fixed.
It still opens an additional file at the 2nd start.
Also with a new workspace.

padawan_0-1695290976676.png

Werner

jhi
Senior

@Semer CHERNI On macos can't type '@' (alt + L) because it is hard coded to 'Login'. At least I can't find it on the list Preferences->General->Keys. Well, it is shown in csv if I export the list, but I can't find it on the list where I can change the bindings.

sh_one
Associate

In 1.13.2, when double-clicking with the mouse to prepare setup data, such as prescaler, a 'c' character often appears in the input box.

sh_one_1-1697850488229.png