2023-11-16 10:36 PM - last edited on 2023-11-20 5:29 AM by Imen.D
I want to use ST-Link OpenOCD to debug and program my STM32H7x board. But always got failure.
My STM32CubeIDE version is STM32CubeIDE_1.13.2, .openocd_2.1.0.202306221132 is within CubeIDE.
The attached is the config file for openOCD(.cfg is not allowed to upload, so I add .log at end of the file). interface/stlink.cfg and target/stm32h7x.cfg should be located to openocd_2.1.0.202306221132/resources/openocd/st_scripts.
When I started debug, I got below information in IDE console. Is there anything I missed or wrong?
Open On-Chip Debugger 0.12.0-00024-gc3ff39f8b (2023-06-26-16:51) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
stm32h7x_cti_prepare_restart_one
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J42S7 (API v2) VID:PID 0483:3748
Info : Target voltage: 3.252984
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : clock speed 4000 kHz
Info : stlink_dap_op_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : [STM32H750VBTx.cm7] Cortex-M7 r1p1 processor detected
Info : [STM32H750VBTx.cm7] target has 8 breakpoints, 4 watchpoints
Info : gdb port disabled
Info : starting gdb server for STM32H750VBTx.cm7 on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: timed out while waiting for target halted
Error executing event gdb-attach on target STM32H750VBTx.cm7:
C:/stm32/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.1.0.202306221132/resources/openocd/st_scripts/gdb_helper.tcl:18: Error: TARGET: STM32H750VBTx.cm7 - Not halted
in procedure 'gdb_attach_hook' called at file "C:/stm32/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.1.0.202306221132/resources/openocd/st_scripts/target/stm32h7x.cfg", line 349
in procedure 'first_gdb_attach_hook' called at file "C:/stm32/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.debug.openocd_2.1.0.202306221132/resources/openocd/st_scripts/gdb_helper.tcl", line 18
Info : Device: STM32H74x/75x
Info : flash size probed value 128k
Info : STM32H7 flash has a single bank
Info : Bank (0) size is 128 kb, base address is 0x08000000
Info : New GDB Connection: 1, Target STM32H750VBTx.cm7, state: running
Warn : GDB connection 1 on target STM32H750VBTx.cm7 not halted
Info : accepting 'gdb' connection on tcp/3333
Info : New GDB Connection: 2, Target STM32H750VBTx.cm7, state: running
Warn : GDB connection 2 on target STM32H750VBTx.cm7 not halted
Error: timed out while waiting for target halted
Error executing event gdb-flash-erase-start on target STM32H750VBTx.cm7:
TARGET: STM32H750VBTx.cm7 - Not halted
Error: failed erasing sectors 0 to 0
Error: flash_erase returned -304
Info : dropped 'gdb' connection
Info : dropped 'gdb' connection
shutdown command invoked
2023-11-20 5:44 AM
Hello @HarryXia,
Make sure to recover the board 10 kΩ resistor from R143 and soldered on to R144 as mentioned in the Caution part, in the STM32H750 User manual.
Check also the SMPS/LDO and VOS settings.
Hope this helped!
Imen
2023-11-20 5:04 PM
@Imen.D thaks your reply.
I checked the manual. "recover the board 10 kΩ resistor from R143 and soldered on to R144" should change the BOOT0 pin to 1 instead of 0, and start in System memory for programming to fix the deadlock issue. But my issue should not be deadlock issue. If I use ST-Link (ST-Link GDB server) instead of ST-Link(OpenOCD), I have no any issue.