2024-03-22 06:09 AM
Je suis incapable de déboguer le code sur ma carte STM32WLE5JC. STM32CubeIDE affiche un message d'erreur indiquant que le ST-Link n'est pas connecté. Cependant, le ST-Link est correctement détecté et connecté dans le STM32CubeProgrammer.
Solved! Go to Solution.
2024-03-25 07:03 AM
Hello @Leila_Megdiche and welcome to the Community 🙂,
I've translated your question with a web-based translation tool to increase the chances that you will get an answer from our experts and community members, as the majority communicate in English:
I am unable to debug the code on my STM32WLE5JC board. STM32CubeIDE displays an error message indicating that the ST-Link is not connected. However, the ST-Link is correctly detected and connected in the STM32CubeProgrammer.
Which STM32CubeIDE version are you using?
Could you please take a look at this post: ST link upgrade issue, I think you've encountered the same issue.
I hope this help you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-25 07:03 AM
Hello @Leila_Megdiche and welcome to the Community 🙂,
I've translated your question with a web-based translation tool to increase the chances that you will get an answer from our experts and community members, as the majority communicate in English:
I am unable to debug the code on my STM32WLE5JC board. STM32CubeIDE displays an error message indicating that the ST-Link is not connected. However, the ST-Link is correctly detected and connected in the STM32CubeProgrammer.
Which STM32CubeIDE version are you using?
Could you please take a look at this post: ST link upgrade issue, I think you've encountered the same issue.
I hope this help you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-25 10:28 AM
thank you @KDJEM.1 for your response and I am sorry for the inconvenience of language I totally forgot that I had to write in English.
I'm using the version 1.15.0 of STM32CubeIDE.
I'll try it Thank you.
Leila Megdiche
2024-04-04 06:28 AM
Hi @Leila_Megdiche ,
Has your request been answered?
If you need further clarification, please do not hesitate to share it 🙂.
Thank you.
Kaouthar.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.