2024-05-15 2:20 PM
I downloaded version 1.15.1 of the STM32 IDE, but when I start a new project and select the STM32F103C8T6 as the MCU, the first image appears. However, when I try to update the firmware, it asks for a login, and the second image appears. I have searched in several places and realized that this is an error that can occur since versions 1.12/1.13. I have tried changing the network connections to active provider (native, manual, and direct), but it doesn't work. (I'm not sure how the manual one works, but I also saw that it's not good to keep using manual mode). Does anyone have any suggestions? The same problem occurs in STM32MX, and I have also tried changing the internet connection.
(First image)
(second image)
Solved! Go to Solution.
2024-05-16 10:48 AM
Dear all,
This is an issue some CubeMx/CubeIDE users are facing since yesterday and the issue was escalated internally to be fixed asap. Dedicated teams are working on it.
2024-05-15 9:58 PM
HEY ST YOUR WASTING YOUR CLIENTS PATIENCE AND GOOD WILL WITH BULLS@#T LIKE THIS
This is the second thread I have come across after experiencing the problem myself, meanwhile ST is silent while we waist our time banging our head against a wall trying to fix it, or twiddling our thumbs waiting for the tools to fix there tools - vendor lock in at its finest.
2024-05-15 11:20 PM
I too faced this issue yesterday and filed a ticket, they asked me to update or re-install. Not even asked for any additional debug info. Looks very casual and they know there are issues with login....
2024-05-16 12:38 AM
same, same, login fails and MX didn't generate code and don't even show an error !
2024-05-16 2:31 AM
Here also same MyST login issue. Updating and re-install didn't solve the issue.
2024-05-16 10:20 AM
Been down for two days now... I can log in through the web site, but the CubeIDE will not log in. It hangs and says the network is down. I have no proxy, VPN, or firewall blocks. I am working on a new design and can't generate code from the ioc file if not logged in. I would strongly recommend making login optional for critical tasks and just keep retrying in the background.
NOTE: I had another system that was logging in on its own at startup just fine. I stupily logged out to see if the problem was machine specific and now that system won't log in either.
2024-05-16 10:39 AM
workaround: install CubeIDE 1.12.1
It has no login functionnality and use latest packages.
2024-05-16 10:43 AM
I too support this view. I don't see reason why it needs login at all since it's a free tool. No need for license check. What's the purpose of login at all for updates.
2024-05-16 10:44 AM
I did reinstall with the latest. Then it ask to migrate all old projects.
2024-05-16 10:46 AM
Will it open projets created with newer version?