2021-11-13 6:51 PM
Hello,
I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V2 and is not working with USB Host.
I tried to convert a test project that worked without RTOS, to use RTOS CMSIS_V1 and is working with USB Host.
Should I use CMSIS_V1 only?
Should CMSIS_V2 also work with USB Host?
2021-11-25 11:16 PM
Hello @rtek1000 ,
What kind of error do you observed?
Do you face this issue when using CubeMx for project generation ?
Imen
2021-11-25 11:28 PM
Hello @Imen DAHMEN ,
Did not generate any Debug message for USB Host using RTOS CMSIS V2.
But for RTOS CMSIS V1 it generated the Debug messages normally.
I used the D.C.T.C. Generator from STM32CubeIDE ver. 1.7.0.
Thank you.
2024-04-26 9:40 PM
Hello @Imen DAHMEN, @rtek1000,
Any update on this as I am also facing the same issue.
I am using STM32Cube IDE v1.13 and stm32f746 discovery board, when I am using freeRTOS CMSIS-V1 USB host works very as a MSC host.
But as soon as I shift to CMSIS-V2 and connect the USB to the board the code gets stuck in the infinite loop of xTaskRemoveFromEventList().
But if I do not connect the USB the firmware's other functionalities are performing as intended.
Any inputs are highly appreciated.
Thankyou