2021-04-22 02:38 AM
The 'reset debug' icon was displayed in V1.6.0 but is no longer visible in V1.6.1. Is this a bug in V1.6.1 or a configuration error of mine? The code is running in the Flash, not RAM (as far as I am aware).
Thanks! Mike.
Solved! Go to Solution.
2021-04-22 02:48 AM
Reset debug icon is available if Debug perspective ... maybe you're still relying on C/C++ editing one ?
2021-04-22 02:48 AM
Reset debug icon is available if Debug perspective ... maybe you're still relying on C/C++ editing one ?
2021-04-22 04:23 AM
2021-04-22 04:33 AM
OK, I have now found out how to open the debug perspective and the reset icon has appeared - however, it was not with the other debug icons. I have now been able to move it so all the debug controls are together. It just goes to show that we all learn something new every day!
Thanks to Cartu38 for the suggestion.
Cheers,
Mike.
2021-04-22 04:53 AM
Please tag such post to answered as will help community to dig into valuable material more quickly. Thanks.