‎2021-04-22 02:38 AM
The 'reset debug' icon was displayed in V1.6.0 but is no longer visible in V1.6.1. Is this a bug in V1.6.1 or a configuration error of mine? The code is running in the Flash, not RAM (as far as I am aware).
Thanks! Mike.
Solved! Go to Solution.
‎2021-04-22 02:48 AM
Reset debug icon is available if Debug perspective ... maybe you're still relying on C/C++ editing one ?
‎2021-04-22 02:48 AM
Reset debug icon is available if Debug perspective ... maybe you're still relying on C/C++ editing one ?
‎2021-04-22 04:23 AM
‎2021-04-22 04:33 AM
OK, I have now found out how to open the debug perspective and the reset icon has appeared - however, it was not with the other debug icons. I have now been able to move it so all the debug controls are together. It just goes to show that we all learn something new every day! :smiling_face_with_smiling_eyes:
Thanks to Cartu38 for the suggestion.
Cheers,
Mike.
‎2021-04-22 04:53 AM
Please tag such post to answered as will help community to dig into valuable material more quickly. Thanks.