2024-07-07 11:37 PM - last edited on 2024-07-08 02:01 AM by SofLit
within the SM32 cube Ide After creating a hex file, I noticed that some lines had less data than others due to linker separation. How can I use the stm32 cube ide to add dummy bytes to the memory?
2024-07-08 12:09 AM - edited 2024-07-08 12:12 AM
> that some lines had less data than others
Thats "normal" in a (Intel-)HEX file.
see:
https://developer.arm.com/documentation/ka003292/latest/
>to add dummy bytes to the memory
Why ?
2024-07-08 01:27 AM
In order to extract data from a hex file and write it into memory while working on the bootloader, I must do a remote update. In order to accomplish this, I must write 0xffff in a location where there is less data on the specific lines. I now know that the linker script can be used to change it but not How to do that.