cancel
Showing results for 
Search instead for 
Did you mean: 

Debugger is showing signed value for unsigned char

Guven47
Associate III

Hello guys,

I have a problem like this. How can I fix this problem

Debug_Error.PNG

24 REPLIES 24

I tried what you said but the problem is not solved. Works properly in Keil

I I use version 13.0.2

I tried what you said but it didn't solve the problem.


@Guven47 wrote:

I tried what you said but it didn't solve the problem.


Tried what?

I asked you to attach a minimal project that reproduces the behavior in order to replicate the same behavior from our side.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@Guven47 wrote:

I I use version 13.0.2


Of STM32CubeIDE?

Try the latest version 1.16.1

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@Guven47 wrote:

I I use version 13.0.2


What year was that version released? 2075?

What tools are you using?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
DaveJ
Associate II

You can right on the value field and pick "Cast to Type" and then type e.g. uint32_t or whatever you want. 


@DaveJ wrote:

You can right on the value field and pick "Cast to Type" and then type e.g. uint32_t or whatever you want. 


You're not getting the point. The OP is already showing the variable as uint8_t but the value is showing as negative (-128)

Plus the OP is in Live Expressions and unless you know of a trick, you can't change the type

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Does this also happen in the 'Variables' view?

Yes,it's happening.