2024-07-23 4:32 PM
CubeIDE 1.16.0 and/or CubeMX 6.12.0.
STM32H563 - SPI devices 4, 5, and 6 only support data widths of 8 or 16 bits. IDE/MX have a Data Size dropdown that let you choose 4 - 16 bits. Widths other than 8 or 16 blow up in HAL_SPI_Init when the data width is checked in an assert in stm32h5xx_hal_spi.c line 258.
2024-08-05 7:52 AM - edited 2024-08-05 8:40 AM
Thank you for the information, I confirm the issue that I reported internally.
Internal ticket number: 188120 (This is an internal tracking number and is not accessible or usable by customers).
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.