Hello @Au,The "100m" in the model io100m_ls_xx_xxx refers to the maximum frequency range. If you would like to know more details about the I/O description, you can refer to the Datasheet, specifically Section 4.2 "Pin Description", Table 26 "Legend/A...
Hello @Katherine , Yes, you're right, "high mode" in datasheet correspond to "fast speed".You can refer to AN4803 application note and precisely section 4.2 "Model selector" and you can find that the bit code naming is aligned with the IBIS model.We ...
Hello @JPiet.3,The STM32H745XIH6 is an MCU from TFBGA 240+25 package.Please refer to the datasheet, specifically "8 Ordering information section" for more information. I have attached the Datasheet link.The BSDL of STM32H745XIH6 is already exist in z...
Hello @Cklau,Please find attached IBIS models of STM32WBA (package UFQFPN48 and UFQFPN32). The IBIS models of STM32WBA will be soon available on the web.Thank you.To give better visibility on the answered topics, please click on Accept as Solution on...