2024-05-01 3:28 AM
Hello,
in CubeIDE (MX) RS485-direction switching is only selectable for UART4 and UART5 (by hardware, not by SW-GPIO). According to user manual, it should be possible for all UARTs/USARTs (Pin DE/RTS). Is this feature missing in CubeIDE or is this hardware-feature only available for UART4/5 (manual is incorrect)?
Regards
Steffen
2024-06-06 3:27 AM
Hello @pit0815
First let me thank you for posting.
I will check this issue internally and I will be back to you asap.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-25 3:37 AM
Hello @pit0815
Your detailed explanation is much appreciated.
A ticket 183549 has been submitted to our dev team in order to fix this asap .
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-03 1:52 AM
I can confirm, that for UART7 and USART6, the Checkbox "Hardware Flow Control (RS485)" is missing. For instance, this is how USART11 looks in my project, using the STM32H563RITx:
And this is USART6, which misses the HW-Flowcontrol configuration options:
Are there any news from the ticket you submitted?
2024-09-12 1:22 PM
Any solution, we have the same problem
2024-09-12 1:55 PM
Can't DE be enabled in code, regardless of CubeMX?
JW