cancel
Showing results for 
Search instead for 
Did you mean: 

Code execution fails on power up (STM32H7A3VGT6 with Cube IDE)

K_K
Associate III

 

Hello,

 

I am currently using the STM32H7A3VGT6 along with STM32 Cube IDE for debugging. My code starts properly in debug mode, but when I power cycle the device without the ST link connected, it sometimes executes and sometimes does not. I have turned ON three LEDs in the MX_GPIO_Init() function, but they do not light up when the code execution fails.

To address this, I adjusted the optimization level from -Og (debug) to O1 (level-1), and the code ran as expected without the debugger. However, after a while, the code stopped executing at optimization level O1, prompting me to revert to -Og for it to work properly again.

I have attached the project settings, debug settings, and code initialization for your reference.

CubeIDE version: 1.14.1

 

 

 

int main(void)
{
	/* USER CODE BEGIN 1 */
	/* USER CODE END 1 */

	/* MCU Configuration--------------------------------------------------------*/

	/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
	HAL_Init();

	/* USER CODE BEGIN Init */

	/* USER CODE END Init */

	/* Configure the system clock */
	SystemClock_Config();

	/* Configure the peripherals common clocks */
	PeriphCommonClock_Config();

	/* USER CODE BEGIN SysInit */
#ifdef RELEASE
	DisableIwdgInStopMode();
#endif
	/* USER CODE END SysInit */
	
	/* Initialize all configured peripherals */
	MX_GPIO_Init();
#ifdef RELEASE
 MX_IWDG1_Init();
#endif
	MX_DMA_Init();
	MX_I2C2_Init();
	MX_SPI1_Init();
	MX_FDCAN1_Init();
	PWM_Init();
	MX_USART1_UART_Init(); // must be after read configuration
	MX_USB_DEVICE_Init(); // must be after read configuration
	MX_ADC1_Init();
	MX_ADC2_Init();
	Start_ADC();

	MX_TIM1_Init();

	//Test_Code();
	/* USER CODE BEGIN 2 */
	Key_Init();
	HAL_TIM_OC_Start(&htim1,TIM_CHANNEL_1);
#ifdef POWER_CALC_OLD
	MX_TIM3_Init();
#endif
	MX_TIM2_Init();

	// TIM3 for processing 5 ADC samples of each channel at 500usec
#ifdef POWER_CALC_OLD
	HAL_TIM_Base_Start_IT(&htim3);
#endif
	/* USER CODE BEGIN 2 */
	Start_CAN();	
while(1)
{

}
}

 

 

image.pngimage.png

 

I would appreciate any assistance you can provide.

Thank you!

9 REPLIES 9
SofLit
ST Employee

Hello @K_K ,

Are you sure it's not the watch dog causing the behavior?

Start with a very simple project by toggling a LED, do you have the same behavior?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
K_K
Associate III

Hello @SofLit 

Yes, I am sure that the issue is not related to the watchdog, as this problem arises when I power up the board, and the code fails to reach the MX_GPIO_Init() line.

Additionally, I have tested a simple program and did not encounter this issue. I have already compared the project settings of both codes, and they are identical.

One observation is that I maintain revisions by copying and pasting the entire code folder. This problem typically occurs when I change the folder name and import it at IDE startup.

For example, when I rename my code folder from 0.0.1 to 0.0.2, I start encountering issues. I do clean, refresh, and rebuild everything after the import.

Thanks!


@K_K wrote:

For example, when I rename my code folder from 0.0.1 to 0.0.2, I start encountering issues.


That's a strange behavior!

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
MM..1
Chief III

Hmm seems more as hw not sw trouble. 1. BOOT pins is managed right ? 2. HSE is managed right ?


@K_K wrote:

 I have turned ON three LEDs in the MX_GPIO_Init() function, but they do not light up when the code execution fails.


So try lighting LEDs at earlier points in the code - to see where it's actually getting to.

Also have something to tell you when Hard Fault and Error Handler are hit ...

Hi,

I don't see any problem related to hardware and software configuration.

Here are the hardware details:

  1. The BOOT0 pin is connected to GND via a 0-ohm resistor.
  2. The reset pin is pulled up with a 10k resistor and has a 100nF capacitor connected to GND.
  3. The VBAT pin is connected to 3.3V with a 100nF capacitor.
  4. The VCAP is 2.2µF.
  5. HSE 25Mhz crystal, SYSCLOCK = 240Mhz. Code attached.


When the RELEASE macro is disabled, the first function called after clock configuration is MX_GPIO_Init(), and in this function LEDs are initialized very first.

Please let me know if there's anything else I should check.

Thanks

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
	RCC_OscInitTypeDef RCC_OscInitStruct = {0};
	RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

	/*AXI clock gating */
	RCC->CKGAENR = 0xFFFFFFFF;

	/** Supply configuration update enable
	 */
	HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

	/** Configure the main internal regulator output voltage
	 */
	__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);

	while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

	/** Initializes the RCC Oscillators according to the specified parameters
	 * in the RCC_OscInitTypeDef structure.
	 */
	RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
	RCC_OscInitStruct.HSEState = RCC_HSE_ON;
	RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
	RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
	RCC_OscInitStruct.PLL.PLLM = 5;
	RCC_OscInitStruct.PLL.PLLN = 96;
	RCC_OscInitStruct.PLL.PLLP = 2;
	RCC_OscInitStruct.PLL.PLLQ = 10;
	RCC_OscInitStruct.PLL.PLLR = 8;
	RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
	RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
	RCC_OscInitStruct.PLL.PLLFRACN = 0;
	if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
	{
		Error_Handler();
	}

	/** Initializes the CPU, AHB and APB buses clocks
	 */
	RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
			|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
			|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
	RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
	RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
	RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
	RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
	RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
	RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
	RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

	if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
	{
		Error_Handler();
	}
}

/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
	RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

	/** Initializes the peripherals clock
	 */
	PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC|RCC_PERIPHCLK_FDCAN;
	PeriphClkInitStruct.PLL2.PLL2M = 5;
	PeriphClkInitStruct.PLL2.PLL2N = 32;
	PeriphClkInitStruct.PLL2.PLL2P = 4;
	PeriphClkInitStruct.PLL2.PLL2Q = 4;
	PeriphClkInitStruct.PLL2.PLL2R = 2;
	PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_2;
	PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
	PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
	PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL2;
	PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
	if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
	{
		Error_Handler();
	}
}

 

Remove HSE 25M from board, config your sw to HSI and test. If all work OK = your HSE is problem.

Please post the schematic

Please note that this behavior is occurring across all boards.

Schematic attached. 

image.png